You are here: Using the TI‑SmartView™ Emulator > Using Screen Capture

Using Screen Capture

To capture the current page, press Ctrl + J (Mac®: ì + J) on your keyboard or on the emulated handheld. The image is automatically placed in the Clipboard and in the TI‑Nspire™ Screen Capture window. You can paste the image into another application without having to take additional steps. This feature is only available when the TI‑SmartView™ panel is active and the workspace is in Handheld mode.

All other screen capture features work the same way they do in other areas of TI‑Nspire™ software. For more information, see Capturing Screens.

 

© 2006 - 2016 Texas Instruments Incorporated