In PublishView™ documents, use hyperlinks to:
| • | Link to a file |
| • | Link to a website on the Internet |
You can add a hyperlink to an open document or you can convert any text within a text box to a hyperlink. When a hyperlink is added, the formatting of the text is underlined and the font color is blue. You can change the formatting of the hyperlinked text without losing the hyperlink.
If a link is broken, an error message is displayed when you click the link:
| • | Cannot open the specified file |
| • | Cannot open the specified web page |
PublishView™ text boxes support both absolute and relative links.
Absolute links contain the complete location of the linked file and do not depend on the location of the main document.
Relative links contain the location of the linked file relative to the main document. If you have multiple lessons in a single folder and they are all linked using relative addressing, you can move the folder to any other location (another local folder, datashare, flash drive, online) without breaking the links. The links also stay intact if you bundle the documents into a lesson bundle or zip them into a zip file and share them.
Note: The PublishView™ document must be saved before you can insert a relative hyperlink.