You are here: Working with PublishView™ Documents > Printing PublishView™ Documents

Printing PublishView™ Documents

You can print reports, worksheets, and assessments created using the PublishView™ feature. To print a document:

1. Click File > Print.

The Print dialog box opens. A preview of the document is shown on the right side of the dialog box.

2. Select a printer from the menu.

Note: The Print what field is disabled.

3. Select Paper Size from the menu. Options are:
Letter (8.5 x 11 inches)
Legal (8.5 x 14 inches)
A4 (210 x 297 mm)
4. Select or type the number of Copies you want to print.
5. In the Print Range area, select to print all sheets in the document, a range of sheets, or the current sheet only.

Note: By default, top and bottom margins are set to one-inch and are maintained when printing a PublishView™ document. There are no side margins. PublishView™ sheets print just as they appear in the workspace.

6. If needed, select or clear the boxes to:
Print problem breaks and names.
Print headers
Print footers
Print object borders
7. Click Print, or click Save As PDF.

 

© 2006 - 2016 Texas Instruments Incorporated