You are here: Using Question in the Teacher Software > Adding Images to Questions

Adding Images to Questions

You can add images to the Question Text Area of most questions. On some question types, you can add an image in the Student Answer or Suggested Response Area of a question.

Adding images provides a visual aid to help explain the context of the question, or as a background on a graph.

Choose the image from a set of images on your computer, or copy and paste an image from a different application into the Question Text Area. For more information, see Working with Images.

Image Types Available

The following file types can be used in the Question application:

.jpg
.jpeg
.bmp
.png

Note: The transparency feature of .png is not supported. Any transparent .png backgrounds will appear as white.

Adding Images Using the Insert Command

1. Click Insert > Image.

The Insert Image dialogue box opens.

2. Navigate to the location of the image and select it.
3. Click Open.

The image appears in the question.

Adding Images Using the Clipboard

To copy an image to the Clipboard from a TI‑Nspire™ document, image file, or another programme, press Ctrl + C (Mac®:  + C).

To paste the image into the question, press Ctrl + V (Mac®:  + V).

 

© 2006 - 2016 Texas Instruments Incorporated