The following table describes the different inputs used in Lists & Spreadsheet wizards.
Input |
Description |
m0 |
Hypothesized value of the population mean that you are testing. |
s |
The known population standard deviation; must be a real number > 0. |
List |
The name of the list containing the data you are testing. |
Frequency List |
The name of the list containing the frequency values for the data in List. Default=1. All elements must be integers | 0. The frequency values can also be typed as a list, in the format {1, 1, 3, 2}. |
v, Sx, n |
Summary statistics (mean, standard deviation and sample size) for the one-sample tests and intervals. |
s1 |
The known population standard deviation from the first population for the two-sample tests and intervals. Must be a real number > 0. |
s2 |
The known population standard deviation from the second population for the two-sample tests and intervals. Must be a real number > 0. |
List 1, List 2 |
The names of the lists containing the data you are testing for the two-sample tests and intervals. |
Frequency 1, Frequency 2 |
The names of the lists containing the frequencies for the data in List 1 and List 2 for the two-sample tests and intervals. Defaults=1. All elements must be integers | 0. |
v1, Sx1, n1, |
Summary statistics (mean, standard deviation, and sample size) for sample one and sample two in two-sample tests and intervals. |
Pooled |
Specifies whether variances are to be pooled for 2‑Sample t Test and 2‑Sample t Interval. |
p0 |
The expected sample proportion for 1‑Prop z Test. Must be a real number, such that 0 < p0 < 1. |
x |
The count of successes in the sample for the 1‑Prop z Test and 1‑Prop z Interval. Must be an integer | 0. |
n |
The count of observations in the sample for the 1‑Prop z Test and 1‑Prop z Interval. Must be an integer > 0. |
x1 |
The count of successes from sample one for the 2‑Prop z Test and 2‑Prop z Interval. Must be an integer | 0. |
x2 |
The count of successes from sample two for the 2‑Prop z Test and 2‑Prop z Interval. Must be an integer | 0. |
n1 |
The count of observations in sample one for the 2‑Prop z Test and 2‑Prop z Interval. Must be an integer > 0. |
n2 |
The count of observations in sample two for the 2‑Prop z Test and 2‑Prop z Interval. Must be an integer > 0. |
C‑Level |
The confidence level for the interval instructions. Must be | 0 and < 100. If it is | 1, it is assumed to be given as a percent and is divided by 100. Default=0.95. |
RegEQ |
The prompt for the name of the function where the calculated regression equation is to be stored. |