You can copy up to 26 columns and 2500 rows from an Excel® spreadsheet to a Lists & Spreadsheet application.
|
1.
|
Drag to select the values that you want to copy from the Excel® spreadsheet. To copy an entire column, click the column identifier at the top of the column. |
Note: If you select non-contiguous columns in the Excel® spreadsheet, they will be pasted as contiguous columns in Lists & Spreadsheet.
|
2.
|
Use the standard key short-cut for copying a selection. |
Windows®: Press +.
Mac®: Press “+.
|
3.
|
In Lists & Spreadsheet, click the cells where you want the data to be pasted. |
If you are copying a range of cells, they will be pasted so that the upper-left corner of the range is positioned at the selected cell. Any data in those cells in will be overwritten.
Windows®: Press +.
Mac®: Press “+.
Handheld: Press / V.
Note: Categorical data must be enclosed in quotes (“ “) after the data is pasted.