You are here: Working with Lesson Bundles > Managing Lesson Bundles

Managing Lesson Bundles

Use the options menu or the context menu to copy, delete, rename or send a lesson bundle to connected handhelds or laptops. You cannot add a folder to a lesson bundle.

Managing Lesson Bundles in the Documents Workspace

1. Open the Content Explorer, and then right-click the lesson bundle name or click to open the context menu.

2. Click the action you want to perform. If an action is not available, it is dimmed.
Click Open to open the lesson bundle.
Click Up One Level to navigate up a level in the folder hierarchy.
You cannot add a folder to a lesson bundle. If you click New Folder, a new folder is added to the folder where the lesson bundle is stored.
Click New Lesson Bundle to create a new lesson bundle. The new lesson bundle is not added to the existing lesson bundle—it is created in the same folder as the existing lesson bundle.
Click Rename to change the name of the lesson bundle. Press Esc to cancel this action.
Click Copy to copy the lesson bundle to the Clipboard.
Navigate to another folder, and then click Paste to copy the lesson bundle in another location.
Click Delete to delete the lesson bundle. Use caution when deleting a lesson bundle. You should ensure files contained in the bundle are backed up if you need the files for future use.
Select All highlights all files in the open folder. This action does not apply to lesson bundles.
Click Package Lesson to create a .tilb file.
Click Refresh to update the list of files in the open folder.

Managing Lesson Bundles in the Content Workspace

1. Click Local Content in the Resources pane.
2. In the Content pane, navigate to the lesson bundle you want to work with, and then right-click to open the context menu or click to open the menu of options.

3. Select the action you want to perform:
Click Open to open the lesson bundle.
Click Copy to place the lesson bundle file in the Clipboard.
Navigate to a folder on your computer or select a connected handheld, and then right-click and click Paste to place the copied file in a new location.
Click Delete to delete the lesson bundle. Use caution when deleting a lesson bundle. You should ensure files contained in the bundle are backed up if you need the files for future use.
Click Refresh to update the list of files in the bundle.
Click Rename to give the lesson bundle a new name. To cancel this action, press Esc.
To move up a level in the folder hierarchy, click Up a Level.
To add the lesson bundle to the list of shortcuts in Local Content, click Create Shortcut.
To add more files to the lesson bundle, click Lesson Bundles > Add Files to Lesson Bundle.
Click Lesson Bundles > Package Lesson Bundle to create a .tilb file.
Click Send to Connected Handhelds to open Transfer Tool and send the lesson bundle to connected handhelds. (This option is not available in TI‑Nspire™ Navigator™ NC Teacher Software.)

 

© 2006 - 2016 Texas Instruments Incorporated