You are here: Getting Help > Activating Your Software License

Activating Your Software Licence

1. Ensure that your computer is connected to the Internet.
2. From the Help menu, select Activate to open the Texas Instruments Activation Wizard.
3. Click Activate your Licence, and then click Next.

The Complete Software Activation dialogue box opens.

4. Complete the name and email fields, and then select the region where you live if different from the default entry. If you want to receive emails from TI about updates, support and promotions, ensure the tick box is selected.
5. Click Next.

The Activate your software dialogue box opens.

6. Type the licence number.
7. Click Next.

The Licence Agreement dialogue box opens.

8. In the Country field, select your country from the drop-down list if it is different from the default entry.
9. Review the licence agreement, and then select to accept the agreement.
10. Click Activate. The licence number is validated against the TI database to ensure it is valid.

If the licence number is valid, the Successful Activation dialogue box opens. If the licence number is not valid, check to make sure the numbers are entered correctly. If the problem persists, contact TI Support.

11. Click Next to continue, or select Finish to complete the installation with default settings.
12. When prompted, click OK to accept the default location for your TI‑Nspire™ folder. If needed, navigate to the location on your computer where you want to store your TI‑Nspire™ documents and files.
13. Select whether or not to replace any documents that have the same name.

The software launches and the Welcome Screen opens.

 

© 2006 - 2016 Texas Instruments Incorporated