You are here: Getting Started with TI‑Nspire™ Navigator NC Teacher Software > Helping Students Log In

Helping Students Log In

Students using TI‑Nspire™ CX Student Software or TI‑Nspire™ CX CAS Student Software can log in to active classes if they have a user name and password.

Note: For information about how to create a class, start a class, build a class roster, and create a user name and password for each student, see Using the Class Workspace.

There are two ways for students to log in:

Using the class name, which is the preferred method.
Using the host name or IP address. Use this method when:
- Broadcasting multiple addresses (such as wired and wireless) and one address is preferred. If your IT administrator has a preferred address, it will be provided. Otherwise, the host name or any other available IP address can be used.
- The class name does not appear in the Select Class and Login dialog box. This occurs when there is a timing issue between the network sending the class name and software receiving it.
- If there are several classes running at the same time that have identical names, such as "Algebra 1." The student will not know which class to select. Best practice is to append a unique identifier such as the course ID or the teacher name to the class name.
ClosedProviding Students with a Host Name or IP Address
ClosedLogging in Using Class Name
ClosedLogging In Using a Host Name or IP Address

 

© 2006 - 2016 Texas Instruments Incorporated