You are here: Writing Lua Scripts > Editing Scripts

Editing Scripts

To edit an existing script, follow these steps.

1. Open the TI‑Nspire™ or PublishView™ document that contains the script. The page containing the script must be active.
2. Select the page and the work area that contains the script.
3. Click Insert > Script Editor > Edit Script.

The Script Editor opens showing the script. If the selected work area on the page does not contain a script, Edit Script is dimmed.

If the script is password protected, the Password Protected dialog box opens prompting for a password.

4. Make any desired changes.
To designate comments, use double hyphens (--) at the start of each comment line.
To change the title, click Edit > Set Script Title or right-click the title and click Set Script Title.

Notes:

Some nonstandard UTF-8 characters may not be displayed correctly. For these characters, it is highly recommended that you use the string.uchar function.
The print function may yield unexpected results for non–UTF-8 characters.
Some nonprintable characters returned by the on.save function will be discarded.
5. To execute the script, click Set Script.

Any errors are displayed in the Console area in the Tools panel.

6. To view the script application (running script), click Focus Script.

 

© 2006 - 2016 Texas Instruments Incorporated