You are here: Programming > Viewing a Program or Function

Viewing a Program or Function

1. From the Actions menu, click View.

2. If the function or program is a library object, select its library from the Location list.
3. Select the function or program name from the Name list.

The function or program is displayed in a viewer.

4. Use the arrow keys to view the function or program.
5. If you want to edit the program, click Edit.

Handheld: Press e to highlight Edit, and then press ·.

Note: The Edit selection is available only for functions and programs defined in the current problem. To edit a library object, you must first open its library document.

 

© 2006 - 2016 Texas Instruments Incorporated