You are here: Programming > Importing a Program from a Library

Importing a Program from a Library

You can import a function or program defined as a library object into a Program Editor within the current problem. The imported copy is not locked, even if the original is locked.

1. From the Actions menu, click Import.

2. Select the Library Name.
3. Select the Name of the object.
4. If you want the imported object to have a different name, type the name under Import As.

 

© 2006 - 2016 Texas Instruments Incorporated