You are here: Using the Portfolio Workspace > Importing an Item to the Portfolio Workspace

Importing an Item to the Portfolio Workspace

You can import a .tns file from your computer to a student’s Portfolio entry.

1. Click Assignments Summary.
2. Highlight a cell in the student row where you want to import the file.

Note: You can import a file for only one student at a time.

3. Click File > Import Item.

The Open dialog box is displayed.

4. Navigate to the file you want to import and click it.
5. Click Import.

If a file already exists in that cell, you are prompted to confirm the file replacement.

Click Replace to save your imported file over the existing file.
Click Keep Existing to keep the existing file and cancel the import file function.

 

© 2006 - 2016 Texas Instruments Incorporated