When working in the Notes application on a desktop, use the Images option on the Insert menu to add an image to a Notes page.
Note: The option for inserting an image is not available when working on a handheld. However, you can transfer a file containing an image from your computer to a TI‑Nspire™ CX handheld.
| 1. | Click Insert > Image from the Documents Toolbar. |
The Insert Image window opens.
| 2. | Navigate to the folder where the image is located. |
| 3. | Select the image, and then click Open to insert the image into the Notes work area. Valid files types are .jpg, .png, or .bmp. |
| 4. | To type text around the image, place the cursor in front of the image or after the image, and then type the text. |
Complete the following steps to resize an image.
| 1. | Click the image to select it. |
| 2. | Move the pointer to the edge of the image. |
The pointer changes to a left-right arrow symbol.
| 3. | Drag the image to make it smaller or larger. |
For more information, see Working with Images.