The TI‑Nspire™ CX Navigator™ classroom learning system uses both your computer and student handhelds. For you and your students to communicate using the TI‑Nspire™ Navigator™ network, students must log in to the network from their handhelds.
Note: You do not have to log in to communicate with student handhelds; you can use the Transfer Tool to delete files or send files and operating systems to student handhelds. However, if you plan to participate from your handheld during the TI‑Nspire™ Navigator™ class session, then you must log in to the TI‑Nspire™ Navigator™ network from your handheld.
For more information on using a handheld, refer to the handheld guidebooks available at education.ti.com/guides.
Before you log in, make sure these items are ready:
| • | You have created your teacher account in Teacher Preferences. |
| • | You have started a class session on your computer. |
| • | The TI‑Nspire™ handheld is ready for login. (The |
Before your students log in, make sure you complete these items:
| • | Create student accounts. |
| • | Provide students with the class network name, their user names and, if necessary, their passwords. |
| 1. | To log in, do one of the following: |
| • | From the Home screen of your TI‑Nspire™ handheld, select 5:Settings > 5:Login. |
| • | From a screen other than the Home screen, press ~ > 8:Login. |
The last network the wireless client was associated with appears on the handheld screen.
Note: If the handheld is connected to the computer with the USB cable, no network names appear on the screen, and you can continue logging in.
| 2. | If the name of the network that appears is correct, continue with login. If the network is not correct, click Network. |
The handheld screens displays all networks it has been connected to, and also displays other networks within range.
| 3. | Select the network from the list, and then click Connect. |
The login screen shows the connection status and displays the network name when the connection is successful.
| 4. | Type your username and password. |
| 5. | Select Login. |
The Login Successful screen opens.
| 6. | Click OK. |
The icons on the TI‑Nspire™ CX, TI‑Nspire™ CX CAS, TI‑Nspire™, and TI‑Nspire™ CAS handheld screens indicate the communication status between the handheld and the access point, wireless adapter, wireless cradle, or TI‑Navigator™ network. The icons indicate status as follows.
|
Icon |
Status |
Meaning |
|
No icon |
|
If no icon appears on the handheld, the handheld is not searching for an access point. Unattach and reattach the wireless adapter or cradle. |
|
|
Blinking |
The handheld is searching for an access point. |
|
|
Solid |
The handheld has found an access point. |
|
|
Solid |
The handheld is not communicating with the adapter or cradle. Remove the handheld from the adapter or cradle, wait for the icon to disappear, and then reattach the handheld to the adapter or cradle. |
|
|
Blinking |
The handheld is connected to the network and is ready to login. |
|
|
Solid |
The handheld is logged in to the network. |