The wireless cradles work with the TI‑Nspire™, TI‑Nspire™ CAS, TI‑Nspire™ CX and TI‑Nspire™ CX CAS handhelds. To connect the handheld to a cradle, follow these steps.
| 1. | Slide the lock on the back of the cradle to the OFF position. |
| 2. | To attach the handheld, face the screen upward and slide the handheld onto the top of the wireless cradle. Be sure that both sides of the handheld are inserted into both of the side guides. |
| 3. | Press firmly to make a good connection. When properly connected, the handheld appears to be sitting on top of the cradle. |
| 4. | Lock the handheld in place by sliding the lock on the back of the cradle to the ON position. |
| 5. | Insert each cradle into the charging bay. Make sure the LED is amber. |
At the end of the school day, return the wireless cradle to the charging bay and charge them overnight. The cradles are charged when all the
(power status) LEDs are solid green or amber.