You are here: Getting Help > Updating the TI‑Nspire™ Software

Updating the TI‑Nspire™ Software

Update the Software

1. Ensure that your computer is connected to the Internet.
2. Close any open documents.
3. From the Help menu, select Check for Upgrades and Notifications.
If your software is current, a confirmation message appears.
If your software is not current, you are prompted to update.
4. Click Update to download and install the update, or click Close to cancel.

A progress indicator shows the download progress. If you receive a connection error, check your Internet connection and try again.

Note for users updating TI‑Nspire™ Navigator™ Teacher Software or TI‑Nspire™ Navigator™ NC Teacher Software: Your portfolio and class records reside on your computer as a database. Because the new software might have features that are not supported in the old database structure, the old data might need to be converted. When conversion is necessary, a Database Update tool helps you make a backup of the old database. The tool appears during the first startup of the updated software.

Manage Automatic Checking

Automatic checking uses the Internet to check for upgrades each time you open the TI‑Nspire™ software. If your system is not up-to-date, you receive a notification. You can turn automatic checking on or off.

1. From the Help menu, select Check for Upgrades and Notifications.
2. Check or clear the Automatically check for updates check box.
3. Click Close.

 

© 2006 - 2016 Texas Instruments Incorporated