You are here: Getting Help > Running TI‑Nspire™ Diagnostics

Running TI‑Nspire™ Diagnostics

If you have trouble with your software, this option enables you to run a short diagnostics program that will help TI support personnel troubleshoot the problem. You do not need Internet access to run diagnostics; however, Internet access is required to send the log file to TI Support. To run diagnostics:

1. From the Help menu, select Run TI‑Nspire™ Diagnostics.

The Software Diagnostic Tool dialog box opens.

2. Click Start to run the program.

The log file is created and the Save as dialog box opens.

3. Navigate to the folder where you want to save the file, and then click Save As.

The Diagnostic Report dialog box opens providing the name of the zip file created and the location where it was saved.

4. Click OK.
5. From the Software Diagnostic Tool dialog box:
Click Send to TI to send the file to TI Support.
Click Restart to run the diagnostics program again.
Click Cancel to quit, and then click OK to confirm and close the dialog box.

 

© 2006 - 2016 Texas Instruments Incorporated