You are here: Graphs Application > Viewing Tables from the Graphs Application

Viewing Tables from the Graphs Application

You can show a table of values for any relation defined in the current problem.

Note: For details about using tables and instructions for accessing tables from the Lists & Spreadsheet application, see Working with Tables.

Showing a Table

From the Table menu, select Split‑screen Table.

The table is displayed with columns of values for the currently defined relations.

To change which relation is displayed in a column, click the arrow in the top cell of the column, and then select the relation name.

Hiding the Table

From the Table menu, select Remove Table.

 

© 2006 - 2016 Texas Instruments Incorporated