You are here: Graphs Application > Specifying a Function with Domain Restrictions

Specifying a Function with Domain Restrictions

You can use the entry line or the Calculator application to specify a function with domain restrictions. For multiple domain restrictions on a function, use the piecewise() function.

In the following example, a function with a domain that is less than 2 and greater than ‑2 is specified on the entry line:

1. From the Graph Entry/Edit menu, select Function.
2. Type the following on the entry line, using spaces to separate the "and" operator:

piecewise(3,x>-2 and x<2)

3. Tap Enter to graph the function.

 

© 2006 - 2016 Texas Instruments Incorporated