You are here: Graphs Application > Graphing Relations

Graphing Relations

Relation graphing is available on Graphs pages and in the Analytic Window of Geometry pages.

You can define relations using , <, =, >, or . The inequality operator () is not supported in relation graphing.

Relation type

Examples

Equations and inequalities equivalent to
y = f(x)

y = sqrt(x)

y-sqrt(x) = 1/2

-2*y-sqrt(x) = 1/2

y-sqrt(x) 1/2

-2*y-sqrt(x) 1/2

Equations and inequalities equivalent to
x = g(y)

x = sin(y)

x-sin(y) = 1/2

x-sin(y) 1/2

Conic equations and inequalities

x^2+y^2 = 5

x^2-y^2 ≥ 1/2+y

Note: Restrictions imposed by an active Press‑to‑Test session may limit the types of relations you can graph.

To Graph a Relation:

1. From the Graph Entry/Edit menu, select Relation.

2. Type an expression for the relation.

3. Press Enter to graph the relation.

Tips for Graphing Relations

You can quickly define a relation from the Function entry line. Position the cursor to the immediate right of the = sign, and then press the Backspace key. A small menu appears with the relation operators and a Relation option. Choosing from the menu places the cursor in the Relation entry line.
You can type a relation as text on a Graphs page and then drag the text object over either axis. The relation is graphed and added to the relation history.

 

© 2006 - 2016 Texas Instruments Incorporated