You are here: Graphs Application > Graphing Equations

Graphing Equations

1. From the Graph Entry/Edit menu, select Equation.
2. Click the type of equation (Line, Parabola, Circle, Ellipse, Hyperbola, or Conic).
3. Click the specific template for the equation. For example, tap y=ax2+bx+c to define a parabola.

The entry line includes a symbol to indicate the type of equation.

4. Type the coefficients into the equation template.

5. Press Enter.

 

© 2006 - 2016 Texas Instruments Incorporated