Using Window/Zoom Tools
Use the Window/Zoom tools to redefine the graph to better view points of interest. The Window/Zoom tools include:
|
•
|
Window Settings: displays a Window Settings dialog box that lets you type the x‑min, x‑max, y‑min, and y‑max values for the axes. |
|
•
|
Zoom - Data: adjusts the zoom factor to display all plotted data. |
|
•
|
Zoom - In: lets you define the center point of the zoom in location. The Zoom In factor is approximately 2. |
|
•
|
Zoom - Out: lets you define the center point of the zoom out location. The Zoom Out factor is approximately 2. |
Using the Window Settings Tool
The dialog box opens. The current values for x‑min, x‑max, y‑min, and y‑max are displayed in the fields.
Note: Only the appropriate boxes are editable, depending on whether there are one or two axes in the work area.
|
2.
|
Type the new values over the old values. |
|
3.
|
Click to apply the changes and redraw the plot. |
Using the Zoom Data Tool
The work area rescales to display all plotted data.
Using the Zoom In Tool
|
2.
|
In the work area, click the center point of the area of interest. This will be the center of the zoom in action. |
The plot redraws to focus and enlarge the portion of the plot centered about the point you selected in the previous step.
Using the Zoom Out Tool
|
2.
|
In the work area, click the center point of the area of interest. This will be the center of the zoom out action. |
The plot redraws to display a larger portion of the plot, centered about the point you selected in the previous step.