You are here: Data Collection > Using Motion Match

Using Motion Match

Use this option to create a randomly generated plot when creating position‑versus‑time or velocity‑versus‑time graphs.

This feature is only available when using a motion detector such as the CBR 2™ sensor or the Go!Motion® sensor.

Generating a Motion Match Plot

To generate a plot:

1. Attach the motion detector.
2. Click View > Graph.
3. Click Analyze > Motion Match.
4. Select one of the following options:
New Position Match. Generates a random position plot.
New Velocity Match. Generates a random velocity plot.

Note: Continue selecting a new position or a new velocity match to generate a new random plot without removing the existing plot.

Removing a Motion Match Plot

To remove the generated plot:

Click Analyze > Motion Match > Remove Match.

 

© 2006 - 2016 Texas Instruments Incorporated