You can select from a variety of sensors and interfaces to collect data while running the Vernier DataQuest™ application with TI‑Nspire™ software.
Multi-channel sensor interfaces let you connect more than one sensor at a time.
|
Description |
|
|
Texas Instruments TI‑Nspire™ Lab Cradle |
This sensor can be used with a handheld, a computer, or as a stand-alone sensor. The sensor interface allows you to connect and use one to five sensors at the same time. It can be used in the lab or at a remote collection location. The Lab Cradle supports two digital sensors and three analog sensors. The Lab Cradle also supports high-sample data collection sensors, such as a hand-grip heart rate or a blood pressure monitor. After using the Lab Cradle as a remote sensor, you can download data to either a handheld or computer. |
Single-channel sensor interfaces can only connect to one sensor at a time. These sensors have either a mini-USB connector for a handheld or a standard USB connector for a computer. For a complete list of compatible sensors, see Compatible Sensors.
|
Description |
||||||||||
|
Vernier EasyLink® |
This sensor interface is used with handhelds. It has a mini-USB connector so it can be plugged directly into the handheld. Connect sensors to Vernier EasyLink® to:
|
|||||||||
|
Vernier Go!Link® |
This sensor interface is used with computers. It has a standard connector so it can be plugged into a Windows® or Mac® computer. Connect sensors to Vernier GoLink® to:
|
| • | Analog sensors. Temperature, light, pH, and voltage sensors are analog sensors and require a sensor interface. |
| • | Digital sensors. Photogates, radiation monitors, and drop counters are digital sensors. These sensors can only be used with the TI‑Nspire™ Lab Cradle. |
| • | Direct-connect USB sensors. These sensors connect directly to a handheld or computer and do not require a sensor interface. |
The following lists some sensors you can use with a handheld.
|
Sensor |
Description |
|||||||||
|
Texas Instruments CBR 2™ |
This analog sensor connects directly to TI‑Nspire™ handhelds through the mini-USB port. It is used to explore and graph motion. This sensor automatically launches the Vernier DataQuest™ application when you connect it to a handheld. Data collection begins when you select the Motion Match function. This sensor collects up to 200 samples per second. Use this sensor to:
|
|||||||||
|
Vernier EasyTemp® temperature sensor |
This analog sensor connects directly to TI‑Nspire™ handhelds through the mini-USB port and is used to collect temperature ranges. You can design experiments to:
|
The following table lists some sensors you can use with a computer.
|
Sensor |
Description |
|||||||||
|
Vernier Go!Temp® temperature sensor |
This analog sensor connects to the computer’s USB port and is used to collect temperature ranges. You can use this sensor to:
|
|||||||||
|
Vernier Go!Motion® motion detector |
This analog sensor connects to the computer’s USB port and is used to measure acceleration, speed, and velocity. Use this sensor to:
|
The following sensors can be used with the Vernier DataQuest™ application.
| • | 25-g Accelerometer |
| • | 30-Volt Voltage Probe |
| • | 3-Axis Accelerometer |
| • | Low-g Accelerometer |
| • | CBR 2™ - Connects directly to handheld USB port |
| • | Go!Motion® - Connects directly to computer USB port |
| • | Extra Long Temperature Probe |
| • | Stainless Steel Temperature Probe |
| • | Surface Temperature Sensor |
| • | Ammonium Ion-Selective Electrode |
| • | Anemometer |
| • | Barometer |
| • | Blood Pressure Sensor |
| • | C02 Gas Sensor |
| • | Calcium Ion-Selective Electrode |
| • | Charge Sensor |
| • | Chloride Ion-Selective Electrode |
| • | Colorimeter |
| • | Conductivity Probe |
| • | High Current Sensor |
| • | Current Probe |
| • | Differential Voltage Probe |
| • | Digital Radiation Monitor |
| • | Dissolved Oxygen Sensor |
| • | Dual-Range Force Sensor |
| • | EasyTemp® - Connects directly to handheld USB port |
| • | EKG Sensor |
| • | Electrode Amplifier |
| • | Flow Rate Sensor |
| • | Force Plate |
| • | Gas Pressure Sensor |
| • | Go!Temp® - Connects directly to computer USB port |
| • | Hand Dynamometer |
| • | Hand-Grip Heart Rate Monitor |
| • | Instrumentation Amplifier |
| • | Light Sensor |
| • | Magnetic Field Sensor |
| • | Melt Station |
| • | Microphone |
| • | Nitrate Ion-Selective Electrode |
| • | O2 Gas Sensor |
| • | ORP Sensor |
| • | pH Sensor |
| • | Relative Humidity Sensor |
| • | Respiration Monitor Belt (Requires Gas Pressure Sensor) |
| • | Rotary Motion Sensor |
| • | Salinity Sensor |
| • | Soil Moisture Sensor |
| • | Sound Level Meter |
| • | Spirometer |
| • | Thermocouple |
| • | TI-Light - Sold only with the CBL 2™ |
| • | TI-Temp - Sold only with the CBL 2™ |
| • | TI-Voltage - Sold only with the CBL 2™ |
| • | Tris-Compatible Flat pH Sensor |
| • | Turbidity Sensor |
| • | UVA Sensor |
| • | UVB Sensor |
| • | Vernier Constant Current System |
| • | Vernier Drop Counter |
| • | Vernier Infrared Thermometer |
| • | Vernier Motion Detector |
| • | Vernier Photogate |
| • | Voltage Probe |
| • | Wide-Range Temperature Probe |