If you are using the TI‑Nspire™ Docking Station or the TI‑Nspire™ CX Docking Station, use this feature to locate handhelds.
1. | Be sure that the handhelds are turned on and that the docking station is connected to your computer. |
2. | Use the Workspace selector to select the Content Workspace. |
3. | Click Tools > Identify Selected Handheld/Lab Cradle. |
Note: You can also right-click the handheld name in the Content pane, and then select Identify Selected Handheld/Lab Cradle.
Both LED lights on the docking station under the slot where the handheld is located will blink for 30 seconds.