You can send a file to all connected handhelds when a class is not in session. To transfer files or folders from a connected handheld or from the computer to all connected handhelds, complete the following steps:
|
1.
|
Use the Workspace selector to select the Content Workspace. |
|
2.
|
Select the files or folders you want to transfer from the Resources pane. |
Note: You can choose files from Computer Content, Web Content, or Connected Handhelds.
|
3.
|
Click , and then click . |
The Transfer Tool window opens.
Note: To add additional files to the transfer list, click .
The selected files and folders are transferred to the connected handhelds. By default, the files are transferred to a folder on the handheld titled Transfers-mm-dd-yy.