Previous TopicNext Topic
You are here: Welcome to the TI‑Nspire™ App for iPad® > Using Variables > Locking and Unlocking Variables

Locking and Unlocking Variables

Locking a variable protects it from modification or deletion, and prevents unintended changes to a defined variable. For example, you may want to lock variables that define time or altitude to ensure integrity.

You cannot lock the following variables:

System variable ans
stat. and tvm. variable groups
Locking Variables

 

1. Go to the Calculator application, and tap the entry line to show the keyboard.
2. Tap Tools .
3. Go to Actions, and then tap Lock.

4. Tap Lock Variable to select the function and insert it into the entry line.
5. Tap , and then tap the variable name you want to lock.

Note: You can also type the variable name in the entry line.

6. Tap ENTER.

The result Done indicates the variable is locked.

Locked variables display a lock icon on the variable menu list.

Note: The Lock command clears the Redo/Undo history when applied to unlocked variables.

Unlocking Variables

 

To modify or delete a locked variable, you must unlock the variable.

1. Tap Tools and go to ActionsLock.
2. Tap Unlock Variable to enter the function into the entry line.
3. Tap , and then tap the locked variable name.
4. Press ENTER to remove the locked status.

The result Done indicates the variable is now unlocked.

 

© 2013-2015 Texas Instruments Incorporated