Previous TopicNext Topic
You are here: Welcome to the TI‑Nspire™ App for iPad® > Lists & Spreadsheet Application > Manual Data Capture

Manual Data Capture

You can use Lists & Spreadsheet application to capture information about objects in the TI-Nspire™ Apps for iPad®. For example, you could track changes of the position of a point on a graph in the Graphs & Geometry application.

The ability to capture data manually is not limited to Graphs & Geometry. This function could work for any other application in the same problem.

Capturing Data Manually
1. Tap the column formula cell (the second cell from the top) of the column in which you want to capture the values.

Note: Captured values replace values in the column.

2. Tap Tools  and go to Data > Data Capture >Manual.

A capture expression is inserted into the column formula cell with "var" as a placeholder for the name of the variable you are capturing.

3. Replace the letters “var” with the name of the variable to capture from Graphs & Geometry. For example, type a or to view a list of available variables, tap var on the TI‑Nspire™ Keyboard.

The formula cell now contains an expression similar to =capture(a,0).

Note: The argument “0” tells Lists & Spreadsheet that you want to trigger each capture manually.

4. Tap Enter.
5. From the Graphs & Geometry application, move the point to a different location where x coordinate of the point is stored in a variable (a, in this example) referenced in the data capture expression.

6. Tap .

The current a value is stored in the Lists & Spreadsheet application configured to capture the variable a.

See Using Variables for more information on adding and using variables.

 

© 2013-2015 Texas Instruments Incorporated