Previous TopicNext Topic
You are here: Welcome to the TI‑Nspire™ App for iPad® > Geometry Application > Creating Geometric Objects

Creating Geometric Objects

You can create objects in both the Geometry and Graphs applications.

Creating Points and Lines

1. Tap Tools , select Points and Lines, and select the type of object, such as Segment. (In the Graphs application, go to Geometry > Points and Lines > Segment.)
2. Tap existing points or locations on the work area to define the object. For example, tap two objects when creating Intersection points.

As you create the object, a tool is shown in the application Toolbar (for example, Segment ). To cancel, tap the X on the tool.

Creating Geometric Shapes

1. Tap Tools , select Shapes, and select the type of object, such as Polygon. (In the Graphs application, go to Geometry > Shapes > Polygon.)
2. Tap existing points or locations on the work area to define the object. For example, tap two locations to define the center and radius of a circle.

As you create a shape, a tool is shown in the application Toolbar (for example, Polygon ). To cancel the shape, tap the X on the tool.

 

© 2013-2015 Texas Instruments Incorporated