Previous TopicNext Topic
You are here: Welcome to the TI‑Nspire™ App for iPad® > Calculator Application > Entering Simple Math Expressions

Entering Simple Math Expressions

Note: To enter a negative number, tap instead of the minus sign.

Suppose you want to evaluate .

1. Tap an entry line in the Calculator work area.
2. Tap to begin the expression.

3. Tap to return the cursor to the baseline.
4. To complete the expression:

Tap .

5. Tap ENTER to evaluate the expression.

The expression is displayed in standard mathematical notation, and result is displayed on the right side of the entry line. If a result does not fit on the same line with the expression, it is displayed on the next line.

The expression and the result are added to the Calculator history.

 

© 2013-2015 Texas Instruments Incorporated