In the TI‑Nspire™ applications that allow formatting, you can use color in filled areas of an object, or in lines or text, depending on the application you are using and how you have selected the item. If the icon or menu item that you want to use is not available (dimmed) after you have selected an item, color is not an option for the selected item.
Colors appear in documents opened on your computer and on the TI‑Nspire™ CX handheld.
Note: For more information about using color in a TI‑Nspire™ application, see the chapter for that application.
To add color to a fill area, line, or text, complete the following steps:
1. | Select the item. |
2. | Click Edit > Color or select where you want to add color (fill, line, or text). |
3. | Select the color from the list. |
To add color using the palette, complete the following steps:
1. | Select the object. |
2. | Click the appropriate toolbar icon. |
3. | Select the color from the palette. |