You are here: Working with TI‑Nspire™ Documents > Creating a New TI-Nspire™ Document

Creating a New TI‑Nspire™ Document

When you open the software, the Documents Workspace opens with a blank document containing one problem. You can add applications and content to this problem to create a document.

Note: The Welcome Screen is displayed when you open the software if the "always show this at startup" option is selected. Click an application icon to add a problem with an active application to a new document.

To create a new document, complete the following steps:

1. On the TI‑Nspire™ File menu,
Select New TI‑Nspire™ Document - Handheld Page Size.

—or—

Select New TI‑Nspire™ Document - Computer Page Size.

The new document opens in the Documents Workspace, and you are prompted to select an application.

2. Select an application to add a problem to the document.

The problem is added to the document.

 

© 2006 - 2015 Texas Instruments Incorporated