The following table describes the toolbar options.
Tool name |
Tool function |
|||||||
|
Suspend Script |
Pauses the script execution. |
||||||
|
Resume Script |
Resumes the script execution. While debugging, the script continues to execute until the next breakpoint or the end of the script. |
||||||
|
Set Script |
Starts the script execution. |
||||||
|
Focus Script |
Sets the focus to the page in the document where the script application is attached:
|
||||||
|
Step Into |
While debugging, executes the current statement. If the statement calls any functions, the debugger stops at the first line of each function. |
||||||
|
Step Over |
While debugging, executes the current statement. If the statement calls any functions, the debugger does not stop within the function unless the function contains a breakpoint. |
||||||
|
Enable Breakpoints |
Switches from normal mode to debugging mode. |
||||||
|
Disable Breakpoints |
Switches back from debugging mode to normal mode and resumes the script. |
||||||
|
Set Permissions |
Sets permission levels to Protected, View Only, or Unprotected and allows you to set a password for the script. |
At the bottom of the window, the Tools panel shows the scripting data. For more information, see the Debugging Scripts section.
Tab |
Window Display |
Console |
Script errors are printed here. Print statements embedded in the script also print here. |
Globals |
Selected global variables are displayed. To select a global variable for display, select Click to add new watch variable at the bottom of the Tools panel. |
Call Stack |
Displays the call tree for the currently executing function. |
Locals |
Local variables in the current function’s scope are displayed. |
Resources |
Upload, insert, and manage images here. |
The status bar at the bottom of the window shows basic script data, as described in this example: stopwatch, 1.1, 4:1, Running.
• | Name of the document that the script application is attached to (stopwatch) |
• | Problem and page number (1.1) |
• | Script line and character, (4:1 describing line 4 and character 1) |
• | Operational state of the script (Running). Note the possible states: |
- | Normal mode: Running, Paused, or Error |
- | Debugging mode: Running (debugging), Paused, or Error |