Setting Script Permissions
You can set permission levels for a script and specify a password to protect a script. Follow these steps.
|
1.
|
In the Script Editor window, click > Set Permissions. |
The Set Permissions dialog box opens.
|
2.
|
In the Permissions Level area, select the appropriate security level: |
|
•
|
Protected. The script can be run, but not viewed or edited. |
|
•
|
View only. The script can be viewed, but not edited. |
|
•
|
Unprotected. The script can be viewed and edited. |
|
3.
|
To secure a script, designate a password in the Security area. |
Note: Use caution when setting passwords because they cannot be recovered.
The next time you click , a Password Protected dialog box opens prompting for the password. Choose one of these options:
|
•
|
To edit the script, enter the password and click . |
|
•
|
To view the script only, do not enter the password and click . |