Setting Minimum API Level
Each release of the T-Nspire™ software includes API support for a specific set of Lua scripting features. Setting the minimum API level for a script lets you specify a minimum set of features that you require for your script.
If a user tries to run the script on a system that does not meet the script's minimum API level, a message notifies the user and prevents the script from running.
To Set the Minimum API Level for a Script:
|
1.
|
Determine the minimum level that you want your script to require. |
|
-
|
Setting the level too low for the script's feature set can result in a script error on older software. |
|
-
|
Setting the level too high can result in the script refusing to start on older software that supports the feature set. |
|
2.
|
On the Script Editor menu, select . |
|
3.
|
In the dialog box, type the minimum level using the format major.minor. For example, you might type 2.3. |
This API level or higher will be required for running the script.