Document settings control how all numbers, including elements or matrices and lists, are displayed in TI‑Nspire™ and PublishView™ documents. You can change the default settings at anytime and you can specify settings for a specific document.
| 1. | Create a new document or open an existing document. |
| 2. | From the TI‑Nspire™ File menu, select Settings > Document Settings. |
The Document Settings dialog box opens.
When you open Document Settings the first time, the default settings are displayed.
| 3. | Press Tab or use your mouse to move through the list of settings. Click ¤ to open the drop-down list to view the available values for each setting. |
|
Field |
Value |
|||||||||
|
Display Digits |
|
|||||||||
|
Angle |
|
|||||||||
|
Exponential Format |
|
|||||||||
|
Real or Complex Format |
|
|||||||||
|
Calculation Mode |
Note: Auto mode shows an answer that is not a whole number as a fraction except when a decimal is used in the problem. Exact mode (CAS) shows an answer that is not a whole number as a fraction or in symbolic form, except when a decimal is used in the problem. |
|||||||||
|
Vector Format |
|
|||||||||
|
Base |
|
|||||||||
|
Unit System (CAS) |
|
| 4. | Click the desired setting. |
| 5. | Choose one of the following options: |
| • | To apply the customized settings to ALL documents, click Make Default. |
| • | To apply the settings to the open document only, click OK. |
| • | To restore default settings, click Restore. |
| • | Click Cancel to close the dialog box without making changes. |