All work that you create and save using TI‑Nspire™ applications is stored as a document, which you can share with others using TI‑Nspire™ software and with those using handhelds. There are two types of documents:
• | TI‑Nspire™ document (.tns file) |
• | PublishView™ document (.tnsp file) |
A TI‑Nspire™ document consists of one or more problems. Each problem can contain one or more pages. A single page is displayed in the work area. All work occurs in the applications within pages.
Because the TI‑Nspire™ software and handhelds share the same functionality, you can transfer TI‑Nspire™ documents between computers and handhelds. When you create a document, you select one of two page sizes.
• | Handheld. Size: 320 × 217 pixels. This size allows documents to be viewed on all platforms. The content will be scaled when viewed on a tablet or larger screen. |
• | Computer. Size: 640 × 434 pixels. The content will not be scaled when viewed on smaller platforms. Some content may not be visible on a handheld device. |
You can convert a document from one page size to the other anytime.
PublishView™ documents can be printed on a standard piece of paper or published to a website or blog. PublishView™ documents can include formatted text, images, and hyperlinks as well as all TI‑Nspire™ applications.
For more information, see Working with PublishView™ Documents