You are here: Working with Images

Working with Images

Images can be used in TI‑Nspire™ applications for reference, assessment, and instructional purposes. You can add images to the following TI‑Nspire™ applications:

Graphs & Geometry
Data & Statistics
Notes
Question, including Quick Poll

In the Graphs & Geometry and Data & Statistics applications, images are set in the background behind the axis and other objects. In the Notes and Question applications, the image is set at the cursor location inline with the text (in the foreground).

You can insert the following image file types: .jpg, .png, or .bmp.

Note: The transparency feature of a .png file type is not supported. Transparent backgrounds are displayed as white.

 

© 2006 - 2014 Texas Instruments Incorporated