Note: Rescaling in the Graphs application affects only the graphs, plots, and objects that reside in the Graphing view. It has no effect on objects in the underlying Plane Geometry view.
▶ | To rescale the x and y axes proportionally, pinch the work area. |
▶ | To rescale only one axis, tap Tools ![]() |
▶ | Tap Tools ![]() |
1. | In the Graphs application, tap Tools ![]() |
2. | Tap Dot Grid, Lined Grid, or (if the grid is already displayed) No Grid. |
1. | Tap either axis to select the axes. |
2. | Tap the Inspector ![]() |
3. | Select the items to change. Changes are applied as you select them. |