Previous TopicNext Topic
You are here: Welcome to the TI‑Nspire™ App for iPad® > Getting Started > Managing Folders

Managing Folders

In the TI‑Nspire™ App for iPad®, management of folders is completed on the Home screen.

Opening Folders
▶ Tap the folder icon to open a folder.
• When you open a folder, all documents within the folder are displayed.
• Tap a document icon to open a document within the folder.
• Tap the folder to close the folder without opening any of the documents.
Adding New Folders

 

1. Tap Add , and then tap Folder.

2. To name the folder, tap the default name assigned to the folder.
3. Type a new name and tap return.

Note: Folders can contain documents, but cannot contain sub-folders.

Creating a Folder with Existing Documents

 

You can also create a new folder by dragging one document onto another document.

 

1. Tap Edit.
2. Drag one document onto another document to create a new folder that contains both documents.
3. Tap Done.
4. Rename the folder if needed.
Renaming Folders

 

1. Tap the default name under the folder.

The keyboard opens.

2. Type a new name, and then tap return.

The new name is displayed and the keyboard closes.

Note: To return to the TI‑Nspire™ Home screen without renaming the item, tap a blank area on the screen.

Deleting Folders

Before you delete a folder, remember that folders may contain several documents. You may want to verify the folder contents before you delete it.

 

1. Tap Edit.
2. Tap on the folder you want to delete.
• Tap Delete to delete the folder.
• Tap Cancel to cancel the delete.
3. Tap Done.

 

© 2013 Texas Instruments Incorporated