Geometry tools are accessible in both the Graphs and Geometry applications. You can use these tools to draw and investigate objects such as points, lines, and shapes.
| • | The Graphing view shows the Graphs work area superimposed on the Geometry work area. You can select, measure, and alter objects in both work areas. |
| • | The Plane Geometry view shows only the objects created in the Geometry application. |
Points, lines, and shapes created in the Graphs application are analytic objects.
| • | All points that define these objects reside on the x,y graph plane. Objects created here are visible only in the Graphs application. Changing the axes scale affects the appearance of the objects. |
| • | You can display and edit the coordinates of any point on an object. |
| • | You can display the equation of a line, tangent line, circle shape, or geometric conic created in the Graphs application. |
|
|
Points, lines, and shapes created in the Geometry application are not analytic objects.
| • | Points that define these objects do not reside on the graph plane. Objects created here are visible in both the Graphs and Geometry applications, but they are unaffected by changes to the Graphs x,y axes. |
| • | You cannot obtain the coordinates of an object’s points. |
| • | You cannot display the equation of a geometric object created in the Geometry application |