You can create objects in both the Geometry and Graphs applications.
| 1. | Tap Tools , select Points and Lines, and select the type of object, such as Segment. (In the Graphs application, go to Geometry > Points and Lines > Segment.) |
| 2. | Tap existing points or locations on the work area to define the object. For example, tap two objects when creating Intersection points. |
As you create the object, a tool is shown in the application Toolbar (for example, Segment
). To cancel, tap the X on the tool.
| 1. | Tap Tools , select Shapes, and select the type of object, such as Polygon. (In the Graphs application, go to Geometry > Shapes > Polygon.) |
| 2. | Tap existing points or locations on the work area to define the object. For example, tap two locations to define the center and radius of a circle. |
As you create a shape, a tool is shown in the application Toolbar (for example, Polygon
). To cancel the shape, tap the X on the tool.