![Previous Topic](../../Data/SkinWHM_iPad_App/ToolbarItem_PreviousTopic.png)
Exploring with Construction Tools
To add a construction, tap
, select , and select the type of construction, such as . (In the Graphs application, go to .)
While a construction is in progress, a tool appears in the application Toolbar (for example,
). To cancel, tap the on the tool.
Midpoint
|
Bisects a segment or sets a midpoint between any two points. The points can be on a single object, on separate objects, or on the work area.
|
Parallel Line
|
Creates a parallel line with respect to any existing line. The existing line can be a Graphs axis or any side of a triangle, square, rectangle, or polygon.
|
Perpendicular Line
|
Creates a line that is perpendicular to a reference line. The reference can be an axis, an existing line, a segment, or one side of a triangle, rectangle, or polygon.
|
Perpendicular Bisector
|
Creates a perpendicular bisector on a segment, on one side of a triangle, rectangle, or polygon, or between any two points.
|
Angle Bisector
|
Creates an angle bisector. The points of the angle can be on existing objects, or they can be locations on the work area.
|
Locus
|
Lets you explore the range of motion of one object with respect to another object as constrained by a shared point.
|
Compass
|
Operates similarly to a geometric compass used for drawing circles on paper.
|