Note: To enter a negative number, tap instead of the minus sign.
Suppose you want to evaluate .
1. | Tap an entry line in the Calculator work area. |
2. | Tap ![]() ![]() ![]() |
3. | Tap ![]() |
4. | To complete the expression: |
Tap
.
5. | Tap ENTER to evaluate the expression. |
The expression is displayed in standard mathematical notation, and result is displayed on the right side of the entry line. If a result does not fit on the same line with the expression, it is displayed on the next line.
The expression and the result are added to the Calculator history.