To open a new document or add a page to an existing document with the Calculator application active:
1. | From the TI‑Nspire™ Toolbar, tap ![]() |
• | If this is a new document, the Add Document menu opens. |
• | If adding a page to an existing document, the Add Page to Document menu opens. |
2. | Tap Calculator ![]() |
The Calculator application is added to the document. By default, the TI‑Nspire™ Keyboard is shown and the cursor is in the entry line.
|
Entry line. Type or insert a math expression in the entry line. Tap ENTER to evaluate the expression.
You can also insert functions, symbols, templates, or expressions from Utilities Note: If the keyboard is hidden, tap the entry line to show it. |
|
Calculator work area. As you evaluate expressions, both the expression and result are saved in Calculator history. To distinguish between each saved expression and result, every other entry line is shaded. To view entry lines that are hidden, drag the work area up or down to scroll. |