DataCollection >> About Vernier DataQuest™ >> Using Vernier DataQuest™ Data in Other TI-Nspire™ Applications

About Vernier DataQuest™

Run the application on either a TI‑Nspire™ handheld or a Windows® or Mac® computer.
Choose from multiple sensor interfaces and sensors, such as the TI‑Nspire™ Lab Cradle, to collect data.
Collect data with up to five connected sensors (three analog and two digital) using the TI‑Nspire™ Lab Cradle. For a complete list of compatible sensors, see Compatible Sensors.

Important: The TI-Nspire™ CM‑C Handheld is not compatible with the Lab Cradle and only supports the use of a single sensor at a time.

Collect data either in the classroom or at remote locations using collection modes such as time-based or event-based.
Select and focus on a subset of collected data.
Collect several data runs for comparison.
Create a graphical hypothesis using the Draw Prediction feature.
Play back the data set to compare the outcome to the hypothesis.
Analyze data using functions such as interpolation, tangential rate, or modeling.
Display results in a graph or a table.
Customize the way results are displayed.
Link the data to other TI‑Nspire™ applications.

Using Vernier DataQuest™ Data in Other TI-Nspire™ Applications

Data obtained during a data collection run is written to the graph and table views in the Vernier DataQuest™ application and can be used in these TI‑Nspire™ applications:

Calculator
Graph
Geometry
Lists & Spreadsheet
Data & Statistics

This graphic shows how data can be shared among the applications.

 

© 2006 - 2012 Texas Instruments Incorporated