DataCollection >> Charging the Lab Cradle >> Charging with an AC Wall Charger

Charging the Lab Cradle

You can charge the Lab Cradle in a number of ways.

Wall charger
USB Cable connected to a computer
TI‑Nspire™ Navigator™ Cradle Charging Bay

Charging with an AC Wall Charger

Connect the plug to a standard AC wall outlet and the mini-B USB connector to the TI‑Nspire™ Lab Cradle.

Charging with a USB Cable

The Lab Cradle can be charged using a standard USB cable. Attach the mini-B connector to the Lab Cradle and the USB type A connector into the computer.

The Lab Cradle will fully charge in less than 12 hours.

Charging with a Charging Bay

Use the TI-Nspire™ Navigator™ Cradle Charging Bay to charge five Lab Cradles at the same time. A full charging bay with dead Lab Cradle units fully charges those units in less than 12 hours.

You can leave the Lab Cradle in the charging bay even if fully charged. You can recharge at any time regardless of the current charge level.

The charging bay is only included in certain bundled packages. The charging bay works with Lab Cradles or with Lab Cradles connected to handhelds.

 

© 2006 - 2012 Texas Instruments Incorporated