Working with TI‑Nspire™ Documents >> Creating a New TI-Nspire™ Document

Creating a New TI-Nspire™ Document

When you open the software, the Documents Workspace opens with a blank document containing one problem. You can add applications and content to this problem to create a document.

Note: The Welcome Screen is displayed when you open the software if the "always show this at startup" option is selected. Click an application icon to add a problem with an active application to a new document.

To create a new document, complete the following steps:

1. Click File > New TI‑Nspire™ Document.

or

Click .

2. Click New TI‑Nspire™ Document.

The new document opens in the Documents Workspace and you are prompted to select an application. By default, new documents open in your current view: computer or handheld. To change the view, use the View menu or click the appropriate icon in the status bar.

3. Select an application to add a problem to the document.

The problem is added to the document.

 

© 2006 - 2012 Texas Instruments Incorporated