Programming >> Creating a Copy of a Function or Program

Creating a Copy of a Function or Program

When creating a new function or program, you might find it easier to start with a copy of the current one. The copy that you create is not locked, even if the original is locked.

1. From the Actions menu, click Create Copy.
2. Type a new name, or click OK to accept the proposed name.
3. If you want to change the access level, select Library Access, and select a new level.

 

© 2006 - 2012 Texas Instruments Incorporated